Column headings on the Labels tab

The following table shows the column headings on the
Labels
tab and their meanings.
Column headings
Descriptions
Version
The number assigned to a file version. Each file version created begins with the number 1. Each additional version, created by checking in or promoting a file or binder, is assigned a sequential number.
Time
The date and time that a label is added to a file or binder.
Label
The descriptive name given to a file version.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal