Device Properties pane

The following table shows the properties in the
Device Properties
pane and their meanings.
Properties
Descriptions
Description
Shows the description of the asset that will be displayed on
Assets
when the asset is selected.
Name
Shows the asset name as it appears in the asset tree. The name is unique within the parent container.
Addressing Info
Shows the asset's location on the control network.
Authentication
Shows the user credentials for the physical device.
This property only applies to the Allen-Bradley E300 Overload Relay assets.
Backup Configuration
Shows the backup settings for the asset.
This property applies to the FactoryTalk Directory and
FactoryTalk® View Site Edition (SE)
assets.
Backup Data
Shows the backup binder or file to use for Backup or Backup and Compare operations for the asset. The Backup Data binder or file is used to store backup files and is used for the compare operations in disaster recovery schedules.
This property applies to Generic FTP devices, Siemens controllers, Mitsubishi controllers, Schneider controllers, Allen-Bradley E300 Overload Relay, Custom Device, Allen-Bradley PowerFlex Drive, Asset Inventory, FactoryTalk Directory, Allen-Bradley Stratix Switch, FactoryTalk View Site Edition,
FactoryTalk® Optix™
Runtime (Embedded), and FactoryTalk Optix Runtime (Software).
Catalog Information
Shows the manufacturer's catalog number for the asset. This box will be filled in when browsing for the addressing information.
Change Detect Capable
Shows the value that the software sets when you browse for the controller in the
Addressing Info
box. If the controller supports and is configured for change detection, then this value is set to
True
. If not, it is set to
False
. If this box is empty, it means that the
Addressing Info
box has not yet been used to browse for the controller.
When this value is set to
False
or blank, the controller is not shown in the list of assets when setting up a Device Monitor - Change Detect schedule.
This property applies to Allen-Bradley Logix 5000 assets.
Configuration Data
Shows the file, folder, or binder that serves as the master file depending on the asset type.
Controller Family
Shows the supported controller family of Siemens S7 Controllers.
This property applies to the Siemens S7 Controller (TIA Portal).
Device Name
Shows the name of the physical asset.
DTM Addressing Info
Shows the asset's location of General DTM Device or Instrument.
This property applies to General DTM Device and Instrument.
It only shows when upgrading from FactoryTalk AssetCentre version 9.00 or earlier if process device capability was activated back then. Starting from FactoryTalk AssetCentre version 10.00, process device capabilities are not supported. If this box was previously configured, it will show "No file selected" upon the upgrade.
Firmware Revision
Shows the firmware revision of the asset.
This property applies to certain asset types, such as Allen-Bradley
SLC™ 500
controllers.
Hardware Revision
Shows the hardware revision or version number of the asset.
Hardware Serial Number
Shows the serial number of the asset. This property shows automatically if the addressing information is valid.
Hardware Type
Shows the asset type.
MAC Address
Shows the MAC Address. This property shows automatically if the addressing information is valid.
This property applies to Allen-Bradley E300 Overload Relay, Allen-Bradley Logix 5000 Controller, Allen-Bradley
MicroLogix™
Controller, Allen-Bradley MobileView, Allen-Bradley
PanelView™
, Allen-Bradley
PanelView Plus
, Allen-Bradley
PLC-5®
Controller, Allen-Bradley SLC 500 Controller, RA Drive, Allen-Bradley PowerFlex Drive, and FactoryTalk Optix Runtime (Embedded).
Manufacturer
Shows the asset manufacturer.
Manufacture Date
Shows the manufacture date of the asset. This property shows automatically if the addressing information is valid.
This property applies to Allen-Bradley E300 Overload Relay, Allen-Bradley Logix 5000 Controller, Allen-Bradley MobileView, Allen-Bradley PanelView, Allen-Bradley PanelView Plus, RA Drive, Allen-Bradley PowerFlex Drive, and FactoryTalk Optix Runtime (Embedded). This property is only retrievable for those devices that are manufactured after the enhanced CIP identity object is introduced.
Operating System
Shows the operating system of the remote computer.
This property applies to remote computers and FactoryTalk Optix Runtime (Software).
Program Name
Shows the name of the Siemens SIMATIC S7 program selected in Configuration Data, along with related information. The format is: Project Name\Station Name\CPU Name\Program Name.
This property applies to Siemens S7 Controller (STEP7).
Scanning Configuration
Shows the scanning properties for Asset Inventory, including:
  • Scan devices using
    CIP™
  • Scan devices using SNMP
  • Scan software using WMI.
This property applies to Asset Inventory.
Security Configuration
Shows the security configuration for the controller.
This property applies to Mitsubishi Controller (GX Works2), Mitsubishi Controller (GX Works3), and FactoryTalk Optix Runtime (Embedded).
Selected Device
Shows the name of the selected Allen-Bradley PowerFlex Drive device.
This property applies to Allen-Bradley PowerFlex Drive.
Series
Shows the series of the asset. This property shows automatically if the addressing information is valid.
This property applies to Allen-Bradley E300 Overload Relay, Allen-Bradley Logix 5000 Controller, Allen-Bradley MicroLogix Controller, Allen-Bradley MobileView, Allen-Bradley PanelView, Allen-Bradley PanelView Plus, Allen-Bradley PLC-5 Controller, Allen-Bradley SLC 500 Controller, RA Drive, Allen-Bradley PowerFlex Drive, and FactoryTalk Optix Runtime (Embedded). This property is only retrievable for those devices that are manufactured after the enhanced CIP identity object is introduced.
TIA Portal Version
Shows the supported TIA Portal version of Siemens S7 Controllers.
This property only applies to the Siemens S7 Controller (TIA Portal).
Warranty Number
Shows the warranty number of the asset. This property shows automatically if the addressing information is valid.
This property applies to Allen-Bradley E300 Overload Relay, Allen-Bradley Logix 5000 Controller, Allen-Bradley MobileView, Allen-Bradley PanelView, Allen-Bradley PanelView Plus, RA Drive, Allen-Bradley PowerFlex Drive, and FactoryTalk Optix Runtime (Embedded). This property is only retrievable for those devices that are manufactured after the enhanced CIP identity object is introduced.
Agent Group
Shows the Agent Group for the asset.
Asset Number
Shows the asset number for management or inventory purposes.
Communication Path
Shows the communication path for General DTM Device or Instrument.
This property applies to General DTM Device and Instrument.
It only shows when upgrading from FactoryTalk AssetCentre version 9.00 or earlier if process device capability was activated back then. Starting from FactoryTalk AssetCentre version 10.00, process device capabilities are not supported.
Location
Shows information about the asset's location in your facility.
Serial Number
Shows the asset's serial number.
Upload Directory
Shows the directory in the robot from which files will be uploaded during a Disaster Recovery operation.
This property applies to ABB Robots.
Backup - Arguments (<ARD>)
Shows the Arguments (<ARD>) for Backup or Backup and Compare schedules.
This property applies to Custom Devices.
Backup - Backup Location
Shows the name for a backup folder, a path to a backup folder, or a path to an existing backup file.
This property applies to Custom Devices.
Backup - Custom Configuration
Shows the configuration information of the custom devices to which you are connected.
This property applies to Custom Devices.
Compare - Arguments (<ARD>)
Shows the Arguments (<ARD>) for comparing operations.
This property applies to Custom Devices.
Compare - Report Location
Shows the file name or path to store the compare report.
This property applies to Custom Devices.
Post Backup - Arguments (<ARD>)
Shows the Arguments (<ARD>) for post backup operations.
This property applies to Custom Devices.
Properties Configuration
Shows the number of extended properties, which could be configured by the
Options dialog: Extended Properties
or configured for a single device.
This property applies to Custom Devices.
Controller I/O Listing
Shows the number of configured I/O modules associated with the Allen-Bradley Logix 5000 Controller, Allen-Bradley MicroLogix Controller, Allen-Bradley PLC-5 Controller, or Allen-Bradley SLC 500 Controller device.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal