Items in the New Label dialog

The following table shows the items in the
New Label
dialog and their meanings.
Items
Descriptions
Allow reuse of existing labels
Select this option to enable the use of a label that has been applied to a previous version of the same file.
Recursively label files and subfolders
Select this option to label all files and files in subfolders within the asset automatically.
This option is only available when you select an asset or a container in the asset tree.
Label
Enter a descriptive name for the file version. The maximum length of a label is 40 characters.
Comments
Enter an optional comment to track work. The maximum length of a comment is 2500 characters.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal