Items in the Get dialog

The following table shows the items in the
Get
dialog and their meanings.
Items
Descriptions
Recursively get files from subfolders
Select this option to retrieve a copy of all files and binders within subfolders of the selected asset, container, or folder to C:\Users\Signed-in User\Downloads on your computer.
This option is only available when you select an asset, a container, or a folder in the asset tree.
Comments
Enter an optional comment to track work. The maximum length of a comment is 2,500 characters.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal