Overview
FactoryTalk® Analytics™ GuardianAI™ is a machine learning based supervisory application that uses existing plant devices, such as variable-frequency drives, as sensors to monitor the health of components such as pumps, fans, and blowers on a plant floor. It uses device data to establish a baseline signature of each component’s behavior under normal operating conditions. Then, it monitors the components for any deviation from the baseline. Once a deviation is detected, a notification is sent to the user identifying the anomaly. If an anomaly is detected but cannot be identified, FactoryTalk Analytics GuardianAI notifies the maintenance engineer that an unidentified anomaly was detected. The engineer can then investigate the issue, determine the cause of the anomaly, and tag the deviation accordingly. FactoryTalk Analytics GuardianAI machine learning engine then trains to identify new anomalies for future encounters. The diagram below illustrates this process and the variation between a known fault and an unknown deviation.
![]() | ![]() |
The FactoryTalk Analytics GuardianAI workflow uses a no-code approach to machine learning. As a result, a data scientist is not required to configure, deploy, or use this AI application. It is designed so that OT personnel, such as maintenance engineers, controls engineers, machine operators, and plant managers, can work with FactoryTalk Analytics GuardianAI with minimal training required.
The configuration workflow consists of four steps:
- Deploy the FactoryTalk Analytics GuardianAI application on an ASEM 6300 industrial computer or a local virtual machine.
- Add the device that will act as a sensor.
- Provide the identifying information about the component being monitored (pump, fan, blower, or motor).
- Training the model to establish the baseline.
FactoryTalk Analytics GuardianAI supports monitoring multiple baselines based on a component's state. Components such as pumps, fans, and blowers on a plant floor can operate under different conditions and processes. FactoryTalk Analytics GuardianAI provides the capability to monitor these varying situations.
NOTE:
State refers to a component's specific operating condition, such as different pressures, flow rates, speed, etc.
FactoryTalk Analytics GuardianAI provides premium integration with the controller to seamlessly read changes in the component’s tags selected during configuration. When a component's tag value in the controller changes, FactoryTalk Analytics GuardianAI automatically creates a new state and starts acquiring the baseline for that specific state. Once the baseline is acquired, FactoryTalk Analytics GuardianAI continuously monitors the component for any deviation in that particular state. FactoryTalk Analytics GuardianAI will automatically switch to the corresponding state based on the change in the controller tags to ensure accurate monitoring.
For example, if a pump operates under different pressures or flow rates, FactoryTalk Analytics GuardianAI will create and monitor baselines for each condition and switch to the appropriate state when the component's operating condition changes to ensure accurate monitoring.
FactoryTalk Analytics GuardianAI application provides premier integration with
PowerFlex® 755, 755TL, 755HiHP, 755TR, 755TM, 755TS, and 6000T drives to use as sensors to
access three-phase current data for motor current signature analysis. It will focus on anomaly
detection and identification for the following component types: pumps, fans, and blowers. The
application is designed to work with single-drive and motor applications. Given its adaptive
nature, FactoryTalk Analytics GuardianAI can learn process-centric issues and adapt to
component types beyond those listed above. For this use case, the application comes equipped
with generic motor control analytics.
Requirements
- Minimum Host Hardware Specifications:
- Processor: Intel Atom 4 Core
- RAM: 8 GB
- SSD: 120 GB
- Recommended Host Hardware Specifications for optimal performance if there are more than 5 components to monitor:
- Processor: Intel i5 and above
- RAM: 16 GB
- SSD: 240 GB
- Host Machine Operating System:
- Linux Debian 11 (or) 12
- Ubuntu 22.04 LTS
- Client Computer:
- Operating System: Windows 10 (or) 11
- Web Browser: Google Chrome (or) Microsoft Edge
- Ensure that the Linux host machine has internet access during installation. Internet access is used during installation to enable the automated script to download dependent packages.
Provide Feedback