Appendix B - Security Considerations
Appendix B provides information about security considerations for FactoryTalk Analytics
GuardianAI.
When deploying FactoryTalk Analytics GuardianAI within operations, considerations should be
applied to the physical and cyber system security posture of the system. The FactoryTalk
Analytics GuardianAI application is designed to run on a client supplied edge hardware and
infrastructure.
System security is a paramount tenet of overall operation success. The following document and
links are being provided as guidance on best practices of how to implement system security
principles within industrial automation control systems. It is considered best practice for
users of FactoryTalk Analytics GuardianAI to follow these practices to provide the best level
of defense in depth security for their overall systems.
Publication Name | Description | Link |
|---|---|---|
Converged Plantwide Ethernet (CPwE) Design | Converged Plantwide Ethernet Design Implementation Guide | |
Deploying Firewalls within CPwE Architecture | Use cases for designing, deploying, and managing industrial firewalls | |
Deploy Identity and Mobility Services | Guidelines for protecting systems through deploying centrally managed defense in-depth security approach | |
Secure Cloud Connectivity to CPwE | Application guide for securing cloud applications within CPwE Architecture | Secure Cloud Connectivity to CPwE |
Deploy CIP Security within CPwE | Network security use cases for CPwE systems | |
Deploy CIP Security within CPwE | IEC 62443 security architecture use cases and design principles | |
Physical Infrastructure within CPwE Architecture | Use cases for deploying robust physical infrastructure for industrial applications |
Provide Feedback