Key Features

  • No Code
    : FactoryTalk Analytics GuardianAI provides no code machine learning. It puts AI into the hands of OT professionals without the need for data science experience.
  • Existing Devices Act as Sensors
    : Users do not need to purchase additional equipment or sensors to get predictive maintenance insights. Early warnings of potential equipment failures are provided leveraging data already available on the plant floor.
  • Anomaly Identification
    : FactoryTalk Analytics GuardianAI goes beyond anomaly detection. It provides users with context about what type of failure will occur which reduces investigation time and reduces maintenance costs and plant downtime.
  • At the Edge
    : There is no need to send large quantities of raw data to the cloud for analysis. FactoryTalk Analytics GuardianAI trains and runs right at the edge providing real-time predictions and minimizing the total cost of ownership.
  • Controller Connection
    : To connect to a controller and select the tags to define the states of the component operation.
  • Multiple Baselines
    : FactoryTalk Analytics GuardianAI supports monitoring multiple baselines of a component based on its state value coming from the PLC.
  • Operator Notifications
    : FactoryTalk Analytics GuardianAI provides the capability to write back detected anomaly data (deviations and/or failure risks) to the PLC, enabling synchronized communication with the controller. This allows control engineers to implement closed-loop actions based on detected anomalies, while enabling operators to respond appropriately when an anomaly is identified.
  • Health Metrics (KPIs)
    : FactoryTalk Analytics GuardianAI delivers real-time Interface health KPIs for each drive. These KPIs enable users to identify the bottlenecks and take corrective action when needed.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal