Health Metrics
FactoryTalk Analytics GuardianAI health metrics to see the key performance indicators of the
training. The following are the metric available:
- Data buffers received per minute: The rate at which data buffers are received, expressed as data buffers received per minute.
- Data buffers processed per minute: The rate at which data buffers are processed, expressed as data buffers processed per minute.
- Data Buffers rejected per minute: The rate at which data buffers are rejected, expressed as data buffers rejected per minute.
- Deviation events per day: The rate at which deviation events are received, expressed as deviation events received per day.
- Model memory used: Memory size of the model represented in KB.
- Database space used: Database size per drive represented in KB.
- Last data buffer received: This represents the timestamp of the last data buffer received.
Health Metrics

Provide Feedback