Notifications
The notification settings enable FactoryTalk Analytics GuardianAI to connect to an SMTP
server to send notification emails when a deviation or failure risk event has been detected.
The Notifications workspace includes:
- Ability to turn notifications on or off.
- SMTP Server Information
- Mailing list configuration to add and remove recipients.
System Setting - Email Notification Configuration

Provide Feedback