General Settings

The general settings allows the user to control additional FactoryTalk Analytics GuardianAI parameters.
  • Timezone
    : Timezones are used to display the timestamps for detected deviations and failure risk events. Rockwell Automation® recommends that the timezone must match the physical location of the compute surface used to host FactoryTalk Analytics GuardianAI.
  • Change Password
    : Users can modify their password to access the application.
  • Certificates
    : Certificates are used to establish the webpage identity for FactoryTalk Analytics GuardianAI. The application comes out of the box with a self-signed certificate. Users have the option to upload their certificates.
General Settings - Application Parameters Configuration
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal