Single Component View

The single component page provides detailed insight regarding deviations and failure risks encountered while monitoring. All new anomalies are displayed as deviations until a user labels the item. Once labeled, a deviation becomes a failure risk.
A failure risk is a previously encountered deviation labeled and confirmed by a user.
The following image displays a deviation. If the component is having multiple states, the deviation and failure risk information particular to current active state will be displayed. Once displayed, the deviation will have a set of First Principle (FP) recommendations for the user to select from.
In the following example, FactoryTalk Analytics GuardianAI detected a deviation with a signature indicating pump cavitation or a fluid viscosity change. If the user determines the deviation is incorrect, they can select normal operation or create a new label.
Users can download the raw data of training, deviation, and failure risk of the drive to analyze the data.
Single Component View with Deviation Detected
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal