Configuration Workspace
The configuration workspace is where users can create folders, add drives, define the
component the drive is powering, and configure the training parameters. The workflow is
designed with an easy-to-use stepper to guide the user in creating a new component for
FactoryTalk Analytics GuardianAI to monitor.
Additionally, controller configuration is available for each folder to read the tags seamlessly and monitor multiple states of the component based on the state value coming from the PLC. The controller configuration is optional.
Configuration Workspace to Add a New Component

Provide Feedback