Resolve Failure Risks

To resolve a failure risk, confirm the corresponding label and click
Mark as Resolved
.
Resolve a Failure Risk
A user can also change the failure risk label and create a new one using the steps illustrated in the deviation workflow section on creating a new deviation label. The user can select the
Other
option and either choose a label from the drop-down or create a new failure risk label.
Upon selecting the existing root cause or creating the new label, the user can associate severity and recommended time to resolve the failure risk (in days). The time to resolve must be in between 1 and 365.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal