Additional Functionalities
In the Single Component View, users can examine all deviations and failure risks associated
with a component operating under various frequencies. If the component functions in multiple
states, each state–frequency combination is represented by a distinct deviation or failure
risk entry. This ensures that users can accurately identify and analyze issues specific to
each operating condition.
Filters
In addition to that, users can apply filters to view the list of deviations and failure
risks. Use filters to narrow down the list by timestamp range, type, first principle,
severity, or any combination of these. Once the required filters are selected, click
Apply
to view the refined results.Filters

List View Customization
The list view of the deviations and failure risks offers several interactive features that
allow users to tailor the view according to their preferences. Each column in the view has
its own interactive features.
- Sort Ascending/Sort Descending: Sort the column data in alphabetical or numerical order, either from lowest to highest or highest to lowest.
- Pin Column: Fix the position of a column so it remains visible while scrolling horizontally.
- Autosize This Column: Automatically adjust the width of the selected column based on its content.
- Autosize All Columns: Automatically adjust the width of all columns to fit their respective content.
- Choose Columns: Select which columns to display or hide based on user preferences.
- Reset Columns: Restore the default column layout and visibility settings.
Provide Feedback