Email Templates

This topic describes the email templates for single event notification and summary notification.

Single Event Notification

The single event notification is intended to send an immediate notification on any deviation or failure risk regarding a component monitored by FactoryTalk Analytics GuardianAI.
For a
deviation
, the notification contains the information shown in the following image:
Example of Deviation Notification Email
  • Component Name
    : Name of the component given during the first-time configuration.
  • Component Type
    : Pump, Fan, Blower, or Motor Analytics.
  • Folder Name
    : The folder name containing the drive and component combination.
  • Time Detected
    : The time at which the event was detected based on the local time zone of the FactoryTalk Analytics GuardianAI instance.
  • State
    : The state at which the component is operating.
  • Output Frequency
    : The output frequency of the drive.
  • Deviation
    : Name of the deviation
  • Probable Causes
    : First Principle Failure mode recommendations.
  • Total Recurrences
    : The amount of time the deviation has been detected.
For a
failure risk
, the notification contains the information shown in the following image.
Example of Failure Risk Notification Email
  • Component Name
    : Name of the component given during the first-time configuration.
  • Component Type
    : Pump, Fan, Blower, or Motor Analytics.
  • Folder Name
    : The folder name containing the drive and component combination.
  • Time Detected
    : The time at which the event was detected based on the local time zone of the FactoryTalk Analytics GuardianAI instance.
  • State
    : The state at which the component is operating.
  • Output Frequency
    : The output frequency of the drive.
  • Failure Risk
    : The name of the failure risk, this is given during the labeling process for a deviation.
  • Failure Risk Description
    : The description of the failure risk indicates additional details about the detected anomaly.
  • Failure Risk Prescription (if exists)
    : Recommendation regarding the action to take to resolve the failure risk.
  • Severity
    : A ranking of the severity (low, medium, high).
  • Time to Resolve
    : Time expected to resolve the failure risk.
  • Total Recurrence
    : The number of times the failure risk has been detected.

Summary Notification

The summary notification provides a high-level table regarding all unlabeled deviations and unresolved failure risks for all components monitored by FactoryTalk Analytics GuardianAI. The table rows will show the component names, with one row dedicated to each component. The table columns include the count of unresolved Failure Risks ranked by severity, along with the count of unlabeled existing deviations with the last column showing the time stamp of the last detected event. If failure risks are classified as High or Medium severity, detailed information is included in the generated email. For Low severity risks, only the count is provided. Below the table is the enumeration of each component with additional details regarding the detected failure risks and deviations.
Summary Notification
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal