Add or Manage Distribution List

Users can add or manage the list of the recipients in the
Distribution List
. To add recipients, follow the below steps:
  1. From the Distribution List section, click
    Add Email
    .
  2. Provide the
    First Name
    ,
    Last Name
    and
    Email
    details of the recipient and click the save icon. All fields are mandatory.
    The "
    New recipient added
    " message is displayed.
    NOTE: A recipient email address must be unique. Duplicate entries with the same email are not allowed.
Add a Recipient
To edit a specific recipient from the list, click the edit icon next to the corresponding recipient, edit the required details and click the save icon.
To delete a specific recipient from the list, click the delete icon next to the corresponding recipient and then click
OK
.
Manage a Recipient
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal