Configure Time Zone
The time zone setting is used by the application to generate timestamps for deviations and
failure risks within the user experience. These timestamps are also referenced in email
notifications to indicate when anomalies occur. It is recommended to configure the time zone
based on the location where the application is installed, ensuring that all recorded events
reflect the local time of detection.
Select the
Time Zone
field, then choose the appropriate time zone to
update it as needed.General Settings - Time zone Configuration

Provide Feedback