Pump First Principle Failure Modes
The following table contains the first principle failure modes embedded within FactoryTalk Analytics GuardianAI for pumps. Pumps are a specific application of motor analytics. When monitoring a pump, FactoryTalk Analytics GuardianAI will provide a combination of pump and motor failure modes. These may be provided as recommendations during deviation detection based on the matching frequency analysis of the deviation.
Failure Mode Label | Description |
|---|---|
Impeller Unbalance | Pump impeller unbalance refers to an irregular distribution of mass or weight
within the impeller of a centrifugal pump. The impeller is a critical rotating
component in a centrifugal pump responsible for generating the flow of fluid. When
there is an imbalance in the impeller, it means that certain parts of the impeller
are heavier or unevenly distributed compared to others. |
Blade Fault | A pump blade fault refers to a problem or issue that affects the blades of the
impeller in a centrifugal pump. The impeller is a critical component of a
centrifugal pump responsible for generating the flow of fluid by rotating and
creating a centrifugal force that propels the liquid. Pump blade faults can have
various causes and consequences, impacting the pump's performance and
reliability. Here are some common types of pump blade faults:
|
Cavitation | Cavitation in centrifugal pumps is a fluid dynamic phenomenon characterized by the
formation of vapor-filled cavities or bubbles within the pump due to low-pressure
regions in the fluid flow. These cavities or bubbles form when the pressure of the
liquid being pumped drops below its vapor pressure, causing the liquid to vaporize
temporarily. When these vapor bubbles move to regions of higher pressure within the
pump, they collapse or implode, creating shockwaves and intense localized pressure
fluctuations. |
Viscosity Changes | Pump viscosity change refers to a variation in the viscosity (thickness or flow
resistance) of the fluid being pumped by a pump. Viscosity is a crucial property of
liquids that affects their flow characteristics. Viscosity can change due to various factors, including temperature fluctuations,
changes in fluid composition, chemical reactions, and contamination. For example,
many fluids become less viscous (thinner) as they warm up and more viscous (thicker)
as they cool down. |
Change in Fluid Dynamics | A change in fluid dynamics for a centrifugal pump refers to alterations or
variations in the characteristics of the fluid flow within the pump or the
associated piping system. These changes can impact the pump's performance,
efficiency, and overall operation. Here are some key aspects of a change in fluid dynamics for a centrifugal pump:
|
Provide Feedback