Fan and Blower First Principle Failure Modes
The following table contains the first principle failure modes embedded within FactoryTalk Analytics GuardianAI for fans and blowers. Fans and blowers are a specific application of motor analytics. When monitoring a fan or blower, FactoryTalk Analytics GuardianAI will provide a combination of fan/blower and motor failure modes. These may be provided as recommendations during deviation detection based on the matching frequency analysis of the deviation
Failure Mode Label | Description |
|---|---|
Blade Misalignment | Fan blade misalignment refers to a condition in which the blades of a fan, such as
those used in industrial fans, HVAC (heating, ventilation, and air conditioning)
systems, or cooling equipment, are not properly aligned with each other or with the
fan hub. This can lead to reduced airflow and efficiency loss.
|
Blade Unbalance | Fan blade unbalance refers to an irregular distribution of mass or weight in the
blades of a fan, resulting in an uneven distribution of forces as the fan rotates.
This condition can lead to excessive vibration and operational problems in fan
systems, including industrial fans, HVAC (heating, ventilation, and air
conditioning) fans, and other types of air-moving equipment. Fan blade unbalance can occur due to various reasons, including manufacturing
defects, wear and tear, erosion of blade material, damage, or the accumulation of
foreign objects or debris on the blades. |
Blade Wear | Fan blade wear refers to the gradual deterioration or erosion of the surfaces of
the blades in a fan, such as those used in industrial fans, HVAC (heating,
ventilation, and air conditioning) systems, or cooling equipment, due to friction,
abrasion, or other forms of material loss over time. This wear can be caused by
various factors and can lead to several operational issues. |
Loose Blade | A loose blade in a fan refers to a condition where one or more blades of the fan
assembly are not securely attached to the fan hub or rotor. This is a potentially
hazardous situation that can lead to significant operational problems, safety
concerns, and damage to the fan system. Loose blades can result from various factors, including manufacturing defects, wear
and tear, damage to blade attachment mechanisms, improper installation, or the
failure of blade fasteners or hardware. |
Electrical Fault | A fan electrical fault refers to a malfunction or problem within the electrical
components of a fan system, such as those found in industrial fans, HVAC (heating,
ventilation, and air conditioning) fans, or cooling equipment. These electrical
faults can disrupt the fan's operation, impact its performance, and pose safety
risks. Fan electrical faults can occur due to various reasons, including electrical
component wear, manufacturing defects, overheating, electrical surges, loose
connections, insulation breakdown, or damage to electrical components. |
Provide Feedback