Training the Asset Baseline
To start training FactoryTalk Analytics GuardianAI, the asset should be running in normal operation. FactoryTalk Analytics GuardianAI is designed to observe the asset under normal usage and will train models across the various speeds of the operation.
Start Training and Monitoring
Click
Start Training & Monitoring
. The user will see the
progress bar begin to populate as data is acquired from the variable frequency drive.The application will create a new model at each half hertz increment of the operation
speed. The model is automatically switched by reading the command frequency of the drive.
Once the number of training iterations is acquired, the given frequency bucket will
automatically switch from training to monitoring. Multiple frequencies can be trained in
parallel depending on the variability in speed of the application. FactoryTalk Analytics
GuardianAI is designed to switch automatically across frequencies between training and
monitoring.
While the asset is in training, the user will not be able to edit the configuration of
that asset. To make any edits, the user should click
Stop Training &
Monitoring
.Training Baseline Asset Behavior

Stop Training and Monitoring
Stop Training & Monitoring will stop training and monitoring the asset. Once the user
stops training, any frequency bucket in progress will be reset back to 0%. Frequencies that
were already fully trained are preserved and will resume monitoring once the user starts
training again.
A dialogue box will prompt the user to accept the in-progress buckets reset and confirm the action.
Stop Training Dialog Box

The user should stop training to make any edits to the drive configuration.
Re-train Asset
Re-training an asset can be important if a major physical change is made to the system.
An example might be replacing the motor or full re-alignment of a coupling. FactoryTalk
Analytics GuardianAI starts the training process under normal conditions, but it is possible
there was already existing degradation at the time the baseline was acquired. In this
scenario, the application will monitor further degradation from baseline. If a user makes a
major physical change without re-training, there is a possibility that FactoryTalk Analytics
GuardianAI will view normal operation as anomalous behavior. If too many false positives are
detected after a major maintenance event, then FactoryTalk Analytics GuardianAI should be
re-trained to acquire a new baseline of the asset’s behavior.
Provide Feedback