System Settings Workspace
The Settings workspace allows the user to control additional parameters of FactoryTalk Analytics GuardianAI.
- Timezone: Timezones are used to display the timestamps for detected deviations and failure risk events. Rockwell Automation recommends the timezone to match the physical location of the compute surface used to host FactoryTalk Analytics GuardianAI.
- Change Password: A user can modify their password to the login screen to access the application.
- Certificates: Certificates are used to establish the webpage identity for FactoryTalk Analytics GuardianAI. The application comes out of the box with a self-signed certificate. Users have the option to upload their own certificates.
System Settings - Application Parameters Configuration

Provide Feedback