Single Asset View

The single asset page provides detailed insight regarding deviations and failure risks encountered while monitoring. All new anomalies will first be displayed as a deviation until a user labels the item. Once labeled, a deviation becomes a failure risk.
A failure risk is a previously encountered deviation that has been labeled and confirmed by a user.
The following image displays a deviation. Once displayed, the deviation will have a set of first principle recommendations for the user to select from. In the following example, FactoryTalk Analytics GuardianAI detected a deviation with a signature matching pump cavitation or a fluid viscosity change. If the user believes that the deviation is incorrect, they have the ability to select normal operation or create a new label.
Users can download the raw data of training, deviation and failure risk of a drive to analyze the data.
Single Asset View with Deviation Detected
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal