Monitoring Workspace
The monitoring workspace, displayed in the following figure, provides quick access to the
overall status of the assets monitored by FactoryTalk Analytics GuardianAI.
- The left panel displays the different folders containing the asset.
- When an asset contained in a folder encounters a deviation or failure risk, a tag on the folder illustrates the count of assets encountering those events.
- The quick filters allow the user to get additional insight regarding the assets with a failure risk, deviation requiring labeling or healthy assets (no action required). Upon selecting a filter, only the assets meeting the criteria are displayed.
- The detailed asset page displays all information about the asset that includes the detailed view of deviations or failure risk requiring user action.
Asset Monitoring Workspace

Provide Feedback