Configuration Workspace

The configuration workspace, accessible from the monitoring workspace, is where users can create folders, add drives, define the asset the drive is powering, and configure the training parameters. The workflow is designed with an easy-to-use stepper to guide the user in creating a new asset for FactoryTalk Analytics GuardianAI to monitor.
Configuration Workspace to Add a New Asset
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal