Creating a New Deviation Label

If none of the first principle recommendations apply, a user can choose to create a new label. To do so, a user should select the “Other” radio button and click
+ Add New
.
Other & Add New Deviation Label
A dialogue box is displayed with the fields to create the new failure Risk label. The label includes the name, descriptions, and prescription (optional).
Creating a New Failure Risk
Upon creating the new label, the user can associate severity and recommended time to resolve the deviation (in days). The time to resolve must be in between 1 and 365.
Severity and Time to Resolve
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal