Email Template

This topic describes the email templates for single event notification and summary notification.

Single Event Notification

The single event notification is intended to send an immediate notification on any deviation or failure risk regarding an asset monitored by FactoryTalk Analytics GuardianAI.
For a
deviation
, the notification contains the information, as shown in the following image.
Example of Deviation Notification Email
  • Asset Name
    : Name of the asset given during the first-time configuration.
  • Asset Type
    : Pump, Fan, Blower, or Motor Analytics.
  • Folder Name
    : The folder name containing the drive and asset combination.
  • Time Detected
    : The time at which the event was detected based on the local time zone of the FactoryTalk Analytics GuardianAI instance.
  • Percent above baseline
    : The percentage deviation from baseline.
  • Duration
    : Amount of time the deviation has persisted.
  • Probable Causes
    : First Principle Failure mode recommendations.
  • Number of recurrences
    : The amount of time the deviation has been detected.
For a
failure risk
, the notification contains the information, as shown in the following image.
Example of Failure Risk Notification Email
  • Asset Name
    : Name of the asset given during the first-time configuration.
  • Asset Type
    : Pump, Fan, Blower, or Motor Analytics.
  • Folder Name
    : The folder name containing the drive and asset combination.
  • Time Detected
    : The time at which the event was detected based on the local time zone of the FactoryTalk Analytics GuardianAI instance.
  • Failure Risk Name
    : The name of the failure risk, this is given during the labeling process for a deviation.
  • Failure Risk Description
    : The description of the failure risk indicates additional details about the detected anomaly.
  • Failure Risk Prescription (if exists)
    : Recommendation regarding the action to take to resolve the failure risk.
  • Severity
    : A ranking of the severity (low, medium, high).
  • Time to Resolve
    : Time expected to resolve the failure risk.

Summary Notification

The summary notification provides a high-level table regarding all unlabeled deviations and unresolved failure risks for all assets monitored by FactoryTalk Analytics GuardianAI. The table rows will show the asset names, with one row dedicated to each asset. The table columns include the count of unresolved Failure Risks ranked by severity, along with the count of unlabeled existing deviations with the last column showing the time stamp of the last detected event. Below the table is the enumeration of each asset with additional details regarding the detected failure risks and deviations
Summary Notification
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal