Configure Time Zone

The Time zone is used by FactoryTalk Analytics GuardianAI to set all time stamps for deviations and failure risks in the user experience. Email notifications also reference timestamps to notify the occurrence of those deviations. It is recommended to set the time zone to reflect the location where the FactoryTalk Analytics GuardianAI edge node is installed to reflect the local time at which the anomalies are detected.
General Settings - Time zone Configuration
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal