Data Integrity and Confidentiality
There is no explicit data or configuration that is shared with FactoryTalk Analytics GuardianAI. The only information exchanged between the PowerFlex Drive and FactoryTalk Analytics GuardianAI application is the three electrical phase currents and the electrical frequency. The user of the FactoryTalk Analytics GuardianAI application is responsible for protecting the container runtime environment unless run inside of FactoryTalk Edge Manager edge node (FactoryTalk Edge Manager).
Provide Feedback