Pump First Principle Failure Modes

The following table contains the first principle failure modes embedded within FactoryTalk Analytics GuardianAI for pumps. Pumps are a specific application of motor analytics. When monitoring a pump, FactoryTalk Analytics GuardianAI will provide a combination of pump and motor failure modes. These may be provided as recommendations during deviation detection based on the matching frequency analysis of the deviation.
Failure Mode Label
Description
Impeller Unbalance
Pump impeller unbalance refers to an irregular distribution of mass or weight within the impeller of a centrifugal pump. The impeller is a critical rotating component in a centrifugal pump responsible for generating the flow of fluid. When there is an imbalance in the impeller, it means that certain parts of the impeller are heavier or unevenly distributed compared to others.
Blade Fault
A pump blade fault refers to a problem or issue that affects the blades of the impeller in a centrifugal pump. The impeller is a critical component of a centrifugal pump responsible for generating the flow of fluid by rotating and creating a centrifugal force that propels the liquid. Pump blade faults can have various causes and consequences, impacting the pump's performance and reliability. Here are some common types of pump blade faults:
  1. Erosion: Erosion occurs when the impeller blades gradually wear away due to the abrasive nature of the fluid being pumped. This is particularly common in pumps handling fluids with suspended solids or corrosive properties. Erosion can result in reduced efficiency and flow rates.
  2. Cavitation Damage: Cavitation is a phenomenon that occurs when the pressure of the fluid drops below its vapor pressure, causing the formation and collapse of vapor bubbles near the impeller blades. This can lead to pitting, erosion, or surface damage on the blade tips, reducing their effectiveness.
  3. Cracks or Fractures: Blade cracks or fractures can develop due to factors such as mechanical stress, excessive loads, or manufacturing defects. Cracked or fractured blades can lead to reduced structural integrity and efficiency.
  4. Bending or Distortion: Blades may become bent or distorted due to impacts, excessive forces, or unbalanced loads. This can result in uneven flow and reduced pump performance.
  5. Wear and Tear: General wear and tear can occur over time, causing blade surfaces to lose their smoothness and shape. This can lead to reduced efficiency and increased energy consumption.
  6. Buildup of Deposits: Some fluids may leave deposits on the impeller blades, such as scale or sludge. These deposits can disrupt the flow pattern and reduce pump performance.
Cavitation
Cavitation in centrifugal pumps is a fluid dynamic phenomenon characterized by the formation of vapor-filled cavities or bubbles within the pump due to low-pressure regions in the fluid flow. These cavities or bubbles form when the pressure of the liquid being pumped drops below its vapor pressure, causing the liquid to vaporize temporarily. When these vapor bubbles move to regions of higher pressure within the pump, they collapse or implode, creating shockwaves and intense localized pressure fluctuations.
Viscosity Changes
Pump viscosity change refers to a variation in the viscosity (thickness or flow resistance) of the fluid being pumped by a pump. Viscosity is a crucial property of liquids that affects their flow characteristics.
Viscosity can change due to various factors, including temperature fluctuations, changes in fluid composition, chemical reactions, and contamination. For example, many fluids become less viscous (thinner) as they warm up and more viscous (thicker) as they cool down.
Change in Fluid Dynamics
A change in fluid dynamics for a centrifugal pump refers to alterations or variations in the characteristics of the fluid flow within the pump or the associated piping system. These changes can impact the pump's performance, efficiency, and overall operation.
Here are some key aspects of a change in fluid dynamics for a centrifugal pump:
  1. Flow Rate Change: A common type of change in fluid dynamics involves adjustments to the flow rate of the fluid being pumped. This change can be intentional to meet varying process requirements or unintentional due to fluctuations in demand.
  2. Pressure Variations: Changes in fluid dynamics can manifest as variations in pressure levels within the pump or the associated piping. These variations can result from changes in system resistance, valve positions, or operational adjustments.
  3. Flow Patterns: Alterations in flow patterns or fluid distribution within the pump or the system can affect pump performance. Flow patterns may change due to factors such as impeller wear, blockages, or changes in system configuration.
  4. Fluid Properties: Variations in fluid properties like temperature, viscosity, density, or composition can impact fluid dynamics within the pump. For example, changes in fluid viscosity can affect flow resistance and pump efficiency.
  5. Cavitation or Aeration: Changes in fluid conditions, such as a drop in fluid pressure or an increase in fluid temperature, can lead to cavitation (the formation and collapse of vapor bubbles) or aeration (the introduction of air or gas into the fluid). These phenomena can affect pump performance and reliability.
  6. Flow Reversal: Flow reversal can occur in certain situations, such as during system startup or shutdown, and can affect pump operation and the direction of flow.
  7. Operational Modes: Changes in pump operating modes, such as switching between parallel or series operations in a multi-pump system, can impact fluid dynamics and overall system behavior.
  8. System Changes: Modifications to the overall system design, such as changes in pipe sizes, the addition of control valves, or the introduction of new equipment, can influence fluid dynamics within the pump and the system.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal