Motor Analytics
The following table contains the first principle failure modes embedded within FactoryTalk Analytics GuardianAI for motors. These may be provided as recommendations during deviation detection based on the matching frequency analysis of the deviation.
Failure Mode Label | Description |
|---|---|
Unbalance | Unbalance may present in two ways, overhung or coupled. Consider two scenarios:
|
Shaft Misalignment | Misalignment refers to a condition where the components of a motor system, such as
the motor shaft and the driven equipment (e.g., a pump or a fan), are not properly
aligned with each other. There are several ways misalignment can occur between two
shafts including angular, parallel and, if fitted with a rolling element bearing,
the bearing could be misaligned with the shaft |
Loose Structural Mounting (Soft Foot) | This can be caused by the structural looseness of machine mounting. Distortion of
the base is likely to cause ‘soft foot’ problems |
Mechanical Looseness | Mechanical looseness refers to a condition where the components of a motor system
are not securely fastened or sufficiently connected |
Rotor Rub | Rotor rub refers to a mechanical issue that occurs when the rotor (the rotating
part of an electric motor) comes into contact with the stator (the stationary part
of the motor). A rotor rub can occur in a radial direction at a seal, for example, or in the axial
direction, due to uneven thermal growth between a turbine rotor and its casing. In
any case, it is a rub, either through a complete shaft revolution or just during a
part of a revolution, between rotating and stationary components. |
Ball Bearing Fault | Common types of bearing ball faults in motors include:
|
Inner Race Bearing Fault | The inner race of a bearing is the part of the bearing that directly contacts and
supports the motor shaft. Common types of inner race bearing faults in motors
include:
|
Outer Race Bearing Fault | The outer race of a bearing is the part of the bearing that is stationary and
typically housed in the motor's casing or housing. Common types of outer race
bearing faults in motors include:
|
Bearing Cage Fault | A bearing cage fault, refers to an issue that occurs within the bearing cage, also
known as the bearing retainer or bearing separator, of a ball or roller bearing used
in an electric motor. Common types of bearing cage faults in motors include:
|
Provide Feedback