About
This Guide
This document will
guide the user through the installer that provides step by step
prompts through the installation. Select specific components to
install on the machine that the installer is currently running on.
To install remaining components to a different machine, run the
installer on that machine. Previously installed components on the
same machine will be detected by the installer.
This guide is intended to be used with the
FactoryTalkAnalytics_DataView_Installer-<version>.<build>.exe
file.Provide Feedback