Application notes
The following are the application notes for
FactoryTalk Activation Manager
.Antivirus software might detect FactoryTalk Activation Manager executable file as a
threat
FactoryTalk Activation Manager
executable file as a
threatYour antivirus software might detect the
AutoGetFTA.exe
file as a threat
and cause an error when you activate a license.To avoid this issue, exclude the
AutoGetFTA.exe
file from the virus
scan.For more information, see Knowledgebase Document ID: BF26715 - FactoryTalk Activation: Error creating process.
TIP:
Sign in to your
Rockwell Automation
account to view Knowledgebase
articles.Incorrect quantity of FlexNet Publisher (FNP) concurrent activations
If you get multiple FlexNet Publisher (FNP) Concurrent and Node-Locked activations of the
same feature name, the
Total
column in the Find Available Activations
page
might display incorrect values. To avoid this issue, get only either Concurrent activations
or Node-Locked activations of a given feature name, not both.FactoryTalk Activation Manager version 4.04 supports renewing activations that have
changed type from FlexNet to CodeMeter
FactoryTalk Activation Manager
version 4.04 supports renewing activations that have
changed type from FlexNet
to CodeMeter
In
FactoryTalk Activation Manager
versions 4.04 and later, renewals of activations can include
an activation type change from FlexNet
to CodeMeter
in
addition to the expiration date change.This type change is supported only when the original
FlexNet
activation
is bound to the computer and replaced with a CodeMeter
activation bound to
the computer.For dongles, perform a rehost of the original activation and a get of the renewed
activation for the activation type. For example, a rehost is necessary when:
- Changing from aFlexNetdongle to aCodeMeterdongle
- Changing from aCodeMeterdongle to aFlexNetdongle
- Activation is bound to aFlexNetdongle, aCodeMeterdongle, or aCodeMetercomputer
In
FactoryTalk Activation Manager
versions 4.02 and later, renewals of activations bound to
dongles or computers are supported in which the technology is not changing.FactoryTalk Activation Manager versions 4.03 and earlier do not support renewing
activations that have changed type from FlexNet to CodeMeter
FactoryTalk Activation Manager
versions 4.03 and earlier do not support renewing
activations that have changed type from FlexNet
to CodeMeter
FactoryTalk Activation Manager
versions 4.03 and earlier do not renew activations that have
changed type from FlexNet
to CodeMeter
. Rockwell Automation
recommends installing version 4.06, which supports renewing
activations that have changed type from FlexNet to CodeMeter. If upgrading to version 4.06
is not possible, perform a rehost of the original activation and a get of the renewed
activation for the activation type.Activation sometimes appears as non-renewable
A security setting or some other obstacle might prevent a renewed activation from being
delivered. When this occurs, the
Rockwell Automation
activation database sometimes
flags the activation as renewed, even though you never received it. The activation could be
marked mistakenly as non-renewable.To correct this problem, contact
Rockwell Automation
technical support and request a
reset of the activation status.FactoryTalk Activation Manager versions on client and server should match to support
Subscription Portal License Manager
FactoryTalk Activation Manager
versions on client and server should match to support
Subscription Portal License ManagerIf upgrading either activation servers or clients from
FactoryTalk Activation Manager
4.00 or
earlier, upgrade both the servers and clients to FactoryTalk Activation Manager
4.06 or later. Unavailable activations are listed only on FactoryTalk Activation Manager running on a
server
FactoryTalk Activation Manager
running on a
serverExpired FlexNet activations do not appear on
FactoryTalk Activation Manager
running on client
machines. This behavior is by design, because expired activations cannot be acted upon from
a client machine. On FactoryTalk Activation Manager
running on a server, activations that are
not available, because they have either expired or not yet reached their start date, are
displayed as disabled and show a red icon. Hovering over the icon displays a tooltip that
explains why the row is disabled.Rehost expired activations to remove them from the Find Available display.
Removing CodeMeter server address from search path causes
errors
CodeMeter
server address from search path causes
errorsAfter a CM activation is borrowed, removing the
CodeMeter
server address
from the search path on the Update Activation Search Path
dialog box on the client PC
causes these errors:- The return of the activation fails and this error appears:Borr.010: Server License not found.
- In theBorrow datebox in theReturn Activationstable, this text appears:Start time is not available. The source of the borrowed license may not be available.
Date and time settings must match on client and server computers
To borrow
CodeMeter
activations correctly, the date and time settings of
the client and server computers must match within one minute. If the date and time settings
do not match, unexpected behavior occurs, such as the failure to activate valid
licenses.Borrowing or returning CodeMeter activations generates only client
diagnostic message
CodeMeter
activations generates only client
diagnostic messageBorrowing or returning
CodeMeter
activations generates only a client
diagnostic message. However, borrowing or returning FlexNet Publisher (FNP) activations
generates both server and client diagnostic messages.This is intended behavior.
Updates to server search list
Rockwell Automation
recommends using FactoryTalk Activation Manager
exclusively to make
updates to the server search list. If using CodeMeter
Web Admin to update
the server search list, the updates may not reflect accurately in the FactoryTalk Activation Manager
search list.Remote Desktop Connection to client computer running Windows Server limits return of
activations and activation of products
When using a remote desktop connection to a client computer running a Windows Server
operating system, borrowed
CodeMeter
activations are not displayed, borrowed
activations cannot be returned manually (they are automatically returned when they expire),
and products relying on the borrowed activation cannot be activated. To work around these
limitations, log into the client computer directly. Rockwell Automation
recommends not
using a Windows Server operating system on a computer that uses borrowed activations or
points to a FactoryTalk Activation
server.FactoryTalk Activation Manager is incompatible with Top Server 6 software
FactoryTalk Activation Manager
is incompatible with Top Server 6 softwareFor
FactoryTalk Activation Manager
to operate correctly, Top Server 6 software must be
uninstalled, and the FLEXID_LIBRARY_PATH environment variable must be removed.For more information on this issue, see Knowledgebase Document ID: BF14522 FactoryTalk Activation Manager: FTAManager has stopped
working.
TIP:
Sign in to your
Rockwell Automation
account to view Knowledgebase
articles.VeriSign Universal Root Certification Authority certificate
If the VeriSign Universal Root Certification Authority certificate does not exist on the
local computer, the certificate is installed while installing Rockwell Automation software.
Use Microsoft Management Console (MMC) to view the certificate in
Console Root >
Certificates (Local Computer) > Trusted Root Certification Authorities >
Certificates
.Unattended or silent install
Use command-line parameters to perform an unattended or silent installation of the
software.
Command-line parameters
The following table identifies the installation command-line parameters. Command-line
parameters are case-insensitive. However, if a specified value includes a space, be sure to
enclose the value in quotation marks (for example, "value with spaces").
Parameter | Description |
|---|---|
/Q | One of /Q and /QS is required if /Record is not specified. Installs the product in the silent mode without any user interface. |
/QS | One of /Q and /QS is required if /Record is not specified. Installs the product in the unattended mode without user interaction during
installation, and shows the progress, errors, or complete messages on the user
interface. |
/IAcceptAllLicenseTerms | Required for /Q or /QS. Specifies that you read and acknowledge all license agreements, and agree to
continue the installation. |
/AutoRestart | Optional. If specified, the computer restarts automatically after the
installation if a restart is required to complete the installation. If a restart
is not required, the parameter is ignored. |
/SetupLanguage | Optional. Specifies which language is displayed during the install process. The value must be one of the following:
If this parameter is omitted, the default language is the user or system user
interface language. |
/Record | Optional. Records inputs to a recording file. |
/Playback | Optional. Plays back a recorded file. |
/DisableAutoRenew | Optional. If specified, disables the FactoryTalk Activation Manager from
automatically connecting to the Rockwell Automation Activation service to query
for renewed activations to download. Activations are renewed automatically by
default. |
Examples
The following examples show how to use the installation commands.
- For a silent install with default parameters:
Setup.exe /Q /IAcceptAllLicenseTerms
- For an unattended install with customized parameter:
Setup.exe /QS /IAcceptAllLicenseTerms /AutoRestart /SetupLanguage=CHS
- For launching an install with the /Record parameter to enter record mode:
Setup.exe /Record
- For launching an install with the /Playback parameter to enter playback mode:
Setup.exe /Q /IAcceptAllLicenseTerms /Playback="C:\Filename.rec"
Error codes
The following table identifies the error codes that can be returned by an installation.
Error Code | Value | Description |
|---|---|---|
ERROR_SUCCESS | 0 | Installation completed successfully. |
ERROR_INVALID_PARAMETER | 87 | One parameters is invalid. |
ERROR_INSTALL_USEREXIT | 1602 | Installation cancelled by user. |
ERROR_INSTALL_FAILURE | 1603 | Fatal error during installation. |
ERROR_BAD_CONFIGURATION | 1610 | Configuration data for product corrupt. Contact support personnel. |
ERROR_REBOOT_CONTINUE | 1641 | Restart required to continue installation. |
ERROR_SUCCESS_REBOOT_REQUIRED | 3010 | Restart required to complete installation. After restart, product is successfully
installed. |
ERROR_REBOOT_PENDING | 3012 | Restart pending. Restart computer for installation to continue. |
ERROR_SUCCESS_NOT_APPLICABLE | 3013 | The installation cannot proceed because the products are already installed. |
Provide Feedback