Security tab
How do I open the Security tab?
- Select
. - Select theSecuritytab.
Use the
Security
tab to sign in to or off from FactoryTalk Security
and view the current user. ControlFLASH Plus
uses the FactoryTalk Security
single sign-on feature. Single sign-on signs in as the Windows-linked user currently signed in to the computer. If single sign-on is disabled, a notification message shows at the top of the Flash Devices
tab. Clicking the message opens the Security
tab prompting the user to sign in.You can sign in as another user by signing out and then signing back in.
- To sign out, clickLog off, then no firmware updates can be performed.
- To sign in, enter the user name and password, then clickLog on.
The
Security
tab displays the following permissions of the current user.- Update firmwareUsers with this permission denied cannot perform flash operations.
- Delete firmware revisionUsers with this permission denied cannot delete firmware revisions.
- Product Compatibility and Download Center connection.
- Users with this permission denied have no access to device revision on the Product Compatibility and Download Center.
- Register productsUsers with this permission denied cannot register Rockwell Automation products.
For more information on single sign-on, see the .
FactoryTalk Services Platform
HelpProvide Feedback