Reports tab
How do I open the Reports tab?
- Select
. - Select theReportstab.
Use the
Reports
tab to configure the automatic saving settings for reports of each flash operation, including:- Option to turn on or off the automatic saving.
- Location of the saved report.
With the
Save a report for each flash operation automatically
checkbox selected, a report summarizing the flash result is automatically saved when a flash operation completes.To change the report location, click
Change
. The default location is C:\Users\<Username>\Documents\ControlFLASH Plus\Reports.Provide Feedback