Options tab
How do I open the Options tab?
- Select
. - Select theOptionstab.
Use the
Options
tab to configure Network Latency
.Network latency indicates how much time it takes for a packet of data to transfer from one
designated point to another. The latency is measured by sending a packet to FactoryTalk Linx
that is returned to the sender. The default value is 10 seconds. It is not recommended to
change the value unless the network is slow and FactoryTalk Linx needs more time to send a
response message.
Provide Feedback