General tab
How do I open the General tab?
- Select
. - Select theGeneraltab.
The following table lists the options in the
General
tab and their meanings.Options | Description |
|---|---|
Flash | Uses Flash to configure whether one selected revision will always be applied to all devices of the same type and the default behavior of the Select Revision for All dialog box. |
Let me choose each time (show messages) | When selecting a firmware revision in the Flash To column of the Flash Devices tab, with this option selected, a confirmation dialog box always opens giving you options to decide if you want to apply the revision to all devices of the same type. |
Yes, always select for all devices (do not show messages) | When selecting a firmware revision in the Flash To column of the Flash Devices tab, with this option selected, the selected revision will always be applied to all devices of the same type without showing a confirmation dialog box. |
No, never select for all devices (do not show messages) | When selecting a firmware revision in the Flash To column of the Flash Devices tab, with this option selected, the selected revision will not be applied to other devices of the same type without showing a confirmation dialog box.The confirmation dialog box has a checkbox used to turn off this function. |
Enable enhanced concurrent flashing algorithm | With this checkbox selected, the enhanced concurrent flashing is turned on to flash up to 20 devices regardless of the topology. With this mode turned on, devices in parent/children relationships and the ones connected on Ethernet linear/DLR topologies are also flashed concurrently. This checkbox is selected by default. |
Enable application log for troubleshooting | With this checkbox selected, the default path for application logs appears and ControlFLASH Plus generates logs anytime it is started and stopped.Tip : When application errors occurred during operations, you can view the application logs to find the causes of the errors. |
Sign in | Selects this button to open the Product Compatibility and Download Center sign-in webpage. When you are signed in, the account shows. |
Sign out | Selects this button to sign out of the Product Compatibility and Download Center. |
Provide Feedback