Components on the tab
The following table explains each item on the Manage Favorites tab.
Item | Description |
|---|---|
Favorite Lists | Shows the favorite lists. |
Import | Imports a CFF (ControlFLASH Favorites) file that is exported with one or more favorite lists. If an imported list has the same name as an existing one, the imported list name is appended with a number to ensure uniqueness. |
Export all | Creates a file including all the favorite lists. |
Filter by favorite list | Filters the favorite lists immediately as the text included in the favorite list name is entered. The amount of filtered and all favorite lists shows on the left of the Filter by favorite list box.An orange highlight indicates that a filter is active. |
New Favorite List | Creates a favorite list. |
Add devices | Adds devices to the selected favorite list. |
Copy | Creates a copy of the selected favorite list. |
Export | Creates a file including the selected favorite list. |
Delete | Deletes the selected favorite list. |
Device | Shows the catalog number of the device. |
Firmware Revision | Shows the device's available firmware revisions as found in the monitored folders. The revision column only includes catalog names. Click the revision to select another one for the device in the favorite list. Click to remove the device from the favorite list. |
Provide Feedback
to remove the device from the favorite list.