Flash operation statuses
The following table lists the statuses of flash operations and their meanings.
Status | Description |
|---|---|
Flash finished | A device is flashed successfully. |
Failed | A device is not flashed successfully. |
Transmitting update | A device is being flashed. |
Polling for power-up | ControlFLASH Plus is waiting for the device to power up. |
Pending | The flashing of the device is queued to start later in the flashing schedule. |
Flash interrupted | An interruption occurs to a flash operation. |
Canceled | A flash operation is canceled. |
Provide Feedback