Download Center License Agreement
The following table lists the options in the
Download Center License Agreement
dialog box and their meanings.Option | Description |
|---|---|
Language | Selects the language of the agreement from the Product and Compatibility and Download Center. The default language is English. |
Accept | Selects this button to start the download. |
Decline | Selects this button to cancel the download. Unable to download revision shows in the Status column.Tip : Select Next to continue flashing the devices with local firmware revisions. |
Cancel | Selects this button to return to the start page. |
Provide Feedback