Sign in to the PCDC
When connected to the Internet, sign in to the Product Compatibility and Download Center to download firmware revisions and view firmware revisions' Important Notice.
Prerequisites
- Make sure the currently signed in user has permission to connect to the Product Compatibility and Download Center. For how to configure the connection permission, refer to FactoryTalk Security System Configuration Guide (publication FTSEC-QS001).
To sign in to the Product Compatibility and Download Center
- In the lower left of thewindow, selectControlFLASH PlusSign in.TIP:You can also selectSettings, and then selectSign in.
- On thePCDC Loginwebpage, enter a registered account and its password.
- (optional) To view firmware revisions' Important Notice easily, selectKeep me signed into enable single sign-on.
- SelectSign in.
Provide Feedback