Configure KPI

After adding an Asset or Component, the user needs to configure KPIs.
Perform the following steps to configure KPIs:
  1. After adding an
    Asset
    or
    Component
    , select the
    KPIs
    tab.
  2. Click
    Add
    .
  3. In the
    Basic Details
    tab, set these parameters:
    • Sensor Name
      : Provide the Sensor Name details.
    • Unit of Measure
      : Select the required Unit of Measure from the drop-down list.
    • Data Types
      : Select the required Data Types from the drop-down list.
    • Asset Class
      : By default, the Asset Class is displayed.
    • Configuration Status
      : Select the required status from the drop-down list.
  4. Click
    Next
    .
    Basic Details
  5. In the
    Configure Equation
    tab, perform the following actions:
    • Equation Name
      : Select the required Equation Name from the drop-down list.
    • Version
      : Select the required Version from the drop-down list.
    • Select the required sensor for the variables from the physical/virtual sensor drop-down list.
      NOTE: It helps to map the variables to the physical/virtual sensors.
    • Click
      Next
      .
      Configure Equation
  6. In the
    Configure KPI Limits
    tab, provide the values to the
    LAL
    ,
    MAL
    ,
    HAL
    ,
    LAU
    ,
    MAU
    , and
    HAU
    .
    NOTE: Click the
    Auto-populate limits
    checkbox to add system-generated limits.
  7. Click
    Add
    .
    Configure KPI Limits
    NOTE:
    The user can hover over the
    Alert Type
    to know about the alert types.
    Alert Types
    The KPI is added to the KPIs table and the "
    KPI was added under the asset successfully
    " message is displayed.
Perform the following steps to edit the KPI details:
  1. Select the required KPI checkbox from the KPI table.
  2. Click
    Edit
    and edit the required fields.
  3. Click
    Save
    .
Perform the following steps to delete the KPI details:
  1. Select the required KPI checkbox from the KPI table.
  2. Click
    Delete
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal