What's New
Current Release 2.01.00 - June 2024
Current Release
2.01.00 - June 2024Asset Intelligence is an application that aims to help customers improve the availability and reliability of their critical assets by actively monitoring the Health and Performance of those assets and notifying key stakeholders when action is needed to prevent planned and unplanned downtime.
Asset Intelligence is a Rockwell Automation Software-as-a-Service offering. It is accessible through the FactoryTalk Hub, and the Data Operations platform is FactoryTalk DataMosaix. All data that is needed as input for Health and Performance is available in FactoryTalk DataMosaix, where it can be easily consumed by Asset Intelligence.
Starting with the Mining Industry, pre-built Asset Classes are available for Ball Mills, Compressors, Conveyors, Crushers, Fans, Flotation Cells, Heat Exchangers, Pumps, Thickeners. These Asset Classes will provide users with value out of the box. Users can build out the hierarchy as required, applying Asset Classes to created Assets to shorten the time to value. The pre-defined KPIs, Asset Classes and the ability to define your own Asset Classes, Formulas and KPIs provide additional capability to expand and scale the solution further.
New Features
- Class definitions:
- Ability to create your own Asset and Component definitions.
- Easy to instantiate, and scale across the enterprise.
- Analytics Enhancements:
- Self-onboard assets across any Asset Class.
- Remaining Useful Life and Health Score KPIs for every Component both Pre-Defined and User-Defined. Both KPIs are rolled up to every Asset.
- Added Weighted Average Rollup from Asset Level upwards for Dashboard Setup.
- Added enhancements to Formula Builder to simplify defining your own formulas.
- Enhanced Onboarding Capabilities:
- Automated Application deployment with entitlement.
- Simplified workflows for Data Source Onboarding with Extractor Configuration.
- Simplified workflows to onboard an Asset.
- General Enhancements and bug fixes:
- Various UI enhancements
- Units of Measure phase 1 through drop down selectors.
- User Management Enhancements:
- Added Custom Role definition.
- Added Data Privileges based on Sites and Asset Classes.
- Provide Pre-Defined Asset Classes with deployment:
- Ball Mills, Compressors, Conveyors, Crushers, Fans, Flotation Cells, Heat Exchangers, Pumps, Thickeners.
- Including corresponding common Components to those Assets.
- Including Performance formulas for each Asset.
- CMMS Integration:
- Support for Fiix CMMS
- CMMS Integration Configuration - Create/Edit/Enable/Validate Connection
- CMMS Asset Mapping Configuration - Fiix and Asset Intelligence Asset Map
- CMMS Automated Work Order Tracking
High Level Features
S.No | Features | Description |
|---|---|---|
1 | Dashboards | It helps the user to visualize the KPI health, get the top 5 underperforming asset at all levels, and access the triggered alerts at each node. |
2 | Favorites | It helps the user to have a list of nodes added to favorites for easy access or navigation. |
3 | Compare | It helps the user to compare assets within an asset class and analyze their common and uncommon KPI Health and their component's risk score. |
4 | Underperforming Assets | It helps the user to analyze the top 5/10/20/100 underperforming assets across any level in the hierarchy considering their common KPIs. |
5 | Trending | It helps the user to visualize the Sensors or KPI's health and get useful insights from their data. |
6 | Alerts | It helps the user to navigate to the global alerts page with list of KPI alerts, Sensor fault alerts across all the levels in the hierarchy |
7 | Data Source Onboarding [Configuration] | It helps the user to create FactoryTalk DataMosaix Extractors that simplifies the Data Source Onboarding Process. |
8 | Asset Setup [Configuration] | It helps the user to create an asset hierarchy structure, configure sensors and KPIs at the asset and component level. |
9 | CMMS Integration Setup [Configuration] | It helps the user to integrate Work Order generation by Asset and tracking in the Work Order progress in the CMMS. |
10 | Formula Setup [Configuration] | It helps the user to create User-Defined Formulas and view the Pre-Defined Formulas available. |
11 | Notification Setup [Configuration] | It helps the user to configure notification for an asset or asset group. |
12 | Dashboard Setup [Configuration] | It helps the user to configure default KPIs to be dis played on the cards throughout the application. |
13 | User Management [Configuration] | It helps the user to create roles, manage user access and resources such as asset class and Sites. |
14 | Class Setup [Configuration] | It helps the user to Create, Modify and Delete Asset and Component Classes. |
Known Anomalies
- Bar graph indicators on dashboards show incorrectly when not using 0 to 100 scaling. (3676062)
- New user is not displayed until the User Management Page is reloaded. (3544746)
- On performing multiple changes in the User Management page, the page becomes inactive. Refresh to continue. (3621842)
- Unable to add multiple new users to any role under User Management. Add the users to the roles one by one. (2396653)
- Historical and Active alerts are not displayed. (3385578)
- Onboarding is failed in case of new tenant for any role other than admin. (3129997)
- Existing user cannot access AI production environment until a user role is assigned to them. (3129987)
Provide Feedback