Known Anomalies

  • Bar graph indicators on dashboards show incorrectly when not using 0 to 100 scaling. (3676062)
  • New user is not displayed until the User Management Page is reloaded. (3544746)
  • On performing multiple changes in the User Management page, the page becomes inactive. Refresh to continue. (3621842)
  • Unable to add multiple new users to any role under User Management. Add the users to the roles one by one. (2396653)
  • Historical and Active alerts are not displayed. (3385578)
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal