View individual event properties
Use the
Event0x
view to view event properties for the input devices.To view individual event properties
- On the tab for the device, expandEvents, and then select the extended event.
- In theEvent0xview, view the parameters for the events.
TIP:
To configure event properties, navigate to the
Tag
editor.Provide Feedback