Copy PWM Configuration

Use
Copy PWM Configuration
to copy the Pulse Width Modulation (PWM) configuration from the current output point to additional output points for 1756-OB16IEF/OB16IEFS digital devices.
To copy PWM Configuration
  1. On the tab for the device, expand
    Pulse Width Modulation
    , and then select an individual point.
  2. In
    PointX
    view, select
    Copy PWM Configuration
    .
  3. In
    Copy PWM Configuration
    , select the points to inherit the copied configuration of the current point.
    TIP:
    Use
    Uncheck All Points
    to clear all the checkboxes for the output points.
  4. Select
    OK
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal