Points view (input)
Use the
Points
view to configure the points on 1756-IB16IF digital devices by:- Enabling the Change of State (COS) timestamp for each input point
- Enabling filters per point
- Setting an input filter time
- Latching timestampsTIP:
- Select or clear all checkboxes in a column at once by selecting or clearing the checkbox in the header of each column.
- If the device connection defined inDevice definitiondoes not include timestamp data:
- The column headingEnable Change of State / Timestampchanges toEnable Change of State.
- Latch Timestampsdisappears.
Provide Feedback