Output Logic view

Use the
Output Logic
view to configure the peer outputs for 1756-OB16IEF digital devices. This allows the input from another device to directly control the outputs on the OB16IEF to enable high speed control based upon the inputs, without requiring 1756-controller processing.
TIP:
To use peer output configuration, in the
Device definition
dialog box, set
Connection
to
Peer Ownership
, and
Output Data
to
Data with Peer
.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal