Inputs view

Use the
Inputs
view to configure the inputs for 1756-LSC8XIB8I digital devices by selecting the input points for each counter.
TIP:
Tip:
  • Each of the counter functions can be configured directly with the output tags for real-time control. For more information on the output tags, refer to the
    ControlLogix Low-speed Counter Module User Manual
    , publication
    1756-UM536
    .
  • Select or clear all checkboxes in a column at once by selecting or clearing the checkbox in the header of each column.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal