Invalid path specified or one of the devices not responding
There was a problem communicating with the device. Check if:
- an incorrect slot was configured for the device.
- the device created in the software does not exist on the network at the address specified in the software, or communication to the device was lost.
- the device has a major fault.
- a bridge device was configured for an incorrect slot, it has faulted, or communication to it was lost.
- RSLinx ClassicorFactoryTalk Linxis running.
Provide Feedback