Servers view

Use the
Servers
view to enable and disable the TCP and UDP ports that are used by the device when it acts as a server. EtherNet/IP uses TCP/IP or UDP/IP for communication.
If the device profile is online to a configurable TCP or UDP server, use the settings to:
  • Enable or disable the port.
  • View information about the TCP or UDP port.
  • Refresh communication to obtain the latest port information from the device.
    TIP:
    The information in the
    Servers
    view is only available when online and configurable ports are available.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal